2014-07-02 3:14 PM
Hello,
I had a question of the best way to implement the supplemental +/- 20 VDC *supplemental* supply (i.e., not the +/- 40 VDC main supply). My 40 VDC supply is unregulated. Two thoughts were to use a voltage divider (off of the +/- 40 VDC supply), or even a high-current regulator on the +/- 40 VDC supply. If a voltage divider is acceptable, what is the best way to minimize the static/idling current when the additional power isn't required ?Thank you,Mr. Amalfi #audio-amplifier-tda72942014-07-02 7:51 PM
http://www.st.com/web/catalog/sense_power/FM142/CL1454/SC354/PF224133?s_searchtype=partnumber
# ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.