2022-01-26 2:39 AM
2022-01-26 8:22 AM
Reply below. Thanks you.
2022-01-27 1:13 AM
OK, I'll try to simplify it again:
Operating Temperature aka Operative ambient temperature
Applies when the component is installed in an application circuit and is currently operating.
In this case, the parameters specified in the data sheet under Electrical Characteristics are guaranteed (provided the remaining ambient conditions are also within the permissible range). This is therefore the permissible operating range.
Storage and Junction Temperature:
Are considered to be a statement of what temperature the component will survive, which has absolutely nothing to do with function or with maintaining parameters under that condition.
Specifically:
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.