cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding LM2901 datasheet: Why is there such a big difference of the typical ICC@(VCC=5V and Tamb=25°C) in table 3 and figure 3?

TFuch.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Because of several reasons. One is the structure of this comparator, which was developed more than 40 years ago. The bipolar technology used and the temperature dependency of e.g. the internal constant-current sources also play a role.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.