cancel
Showing results for 
Search instead for 
Did you mean: 

I'm trying to work with STAPI003 audio amplifier, in the datasheet it says that it 4 x 52 W/4 Ω max, but i am not able to get more than 32 watt at 4 ohm. How can i achieve above 32 watt, is it possible to bridge the output?

MDarw.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
MM..1
Chief III
  • 4 x 52 W/4 Ω max.
  • 4 x 30 W/4 Ω @ 14.4 V, 1 kHz, 10 %

How is your Vcc ? For more power you need more Vcc...

MDarw.1
Associate II

Hello,

My Vcc is accurate 14.4V DC with 30amp available current. The supply voltage is not dropping when try to increase the sine wave source input, when the output goes above 32 watt it start clipping. So the maximum stable output i could reach at 4 ohm was 32 watt. Is there any trick for this IC to increase the output level?

I can only repeat trick is more Vcc see docu for max.

MDarw.1
Associate II

How about bridging the outputs, can this IC support this feature?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.