2019-04-24 7:45 AM
How are you?
I would like to test an ultrasound pulser IC evaluation board (STEVAL-IME012V1) on Windows 10 PC. I installed a test software (STSW-IME011) to configure waveforms (frequency and number of pulses) for the evaluation board. However, I have not connected the evaluation board to the Windows 10 PC. The PC has not shown a suitable COM port (USB- 5 pin connection) yet. Would you please show me how to find the evaluation board on the Windows 10 PC?
Actually, I connected only with the 5-pin USB port to the PC. Should I connect power lines to the evaluation board?
Thank your for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.