Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

I2S Basics

Posted on July 05, 2018 at 18:03Hi everyone,I'm looking for some help after many days of pain.I'm trying to write basic uSD to I2S application, but the result is really ugly.I'm using STM3240G eval board and Adafruit MAX98357 board.I'm using fatfs a...

TDA7265B free sample

Posted on April 08, 2018 at 21:30Hi, I need a free sample of TDA7265B. It is a class-AB two-channel power amplifier. I didn't find in a list of free samples of integrated circuits of its class. There is a TDA7265 chip, it is very similar but not the...

STDP6028 - Programming Flash

Posted on July 07, 2018 at 12:17Hi,Trying to program STDP6028,Able to read registers from GProbe tool. But when I try to program Hex file. Tool shows progress of flash write. But after complete, no other prints come on the console. On very reset I w...

CS30 - susceptibility to noise?

Posted on June 22, 2018 at 11:56Placing a CS30A next to a 0.05ohm sense ohm successfully measured output currents from 24v boost converter.Since the microcontroller was not nearby, to reduce noise thought it might be better to place the CS30A next t...

R K by Associate II
  • 1303 Views
  • 4 replies
  • 0 kudos

Inductive load current sensing with CS30.

Posted on June 21, 2018 at 21:44Hello everyone. I would like to know if is possible to use the CS30 current sense amplifier with inductive loads, i.e. something similar to the coils of solenoids used in automatic car gearboxes. Thanks in advance.The...

Resolved! LMX358IQ2T Output Current Capability

Posted on May 03, 2018 at 05:29Hi, I'm looking for an op-amp to buffer a signal and provide an output of 2 -> 5V to a load of 100 - 200R. This would require driving the load with 50 - 100 mA. The LMX358IQ2T has a specified output source current of 6...

usb type-c audio

Posted on June 21, 2018 at 11:14The stm32f429 fs usb then type-c mouth to do the host, then the headset device can achieve this program?

type-c audio

Posted on June 21, 2018 at 11:13stm32f429的fs usb 接type-c��主机,接耳机设备这�方案�以实现�

About bluecoin Beamfoming and Souce Localization

Posted on June 18, 2018 at 09:46Hi. I'm soohoon.I have bluecoin device.I have question.1. Now Beamforming is fixed in the one direction I set,    I want to make automatically BF in the direction of sound.What should I do?2. Now I know souce Localiza...