Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

Resolved! What is a single comparator?

Here is the datasheet :TS881 - Rail-to-rail 0.9V nanopower, push-pull single comparator - STMicroelectronicsDoes it mean I can use it in single power supply with VS- connected to GND?

AMark.2 by Associate
  • 2062 Views
  • 2 replies
  • 0 kudos

AD7768 ADC Data Interface

Hello,I'm working on a data acquisition project and i'm looking to use the AD7768 ADC.The datasheet says it has a 8 channel data interface, but i cant really find out what data protocol it is. Is it just plain data bits? if yes, can i just read it wi...

Is the RHF350A a silicon-germanium (SiGe) opamp?

Hello, I'm searching for a space grade/rad hard, low noise (<5nV/rtHz), high bandwidth opamp (>100 MHz) for cryogenic operation. SiGe opamps are generally known to perform favorably at cryogenic temperatures. At first glance the RHF350A has good spec...

ELivi.1 by Associate
  • 861 Views
  • 0 replies
  • 0 kudos

Input current of the FB pin of ST715

As on the title. The data sheet does not inform this parameter so it is hard to define what is the maximum resistance on the feedback network that will produce an acceptable error.The data sheet informs that resistance R2 (bottom resistance) of the f...

ECost by Associate II
  • 1045 Views
  • 0 replies
  • 0 kudos

TS9222_Stability_Analysis

Hi, I have an amplifier circuit build using TS9222 opamp, with gain = 40 and external EMI filter on the inputs. I want to understand the affect of filter capacitors at the input of opamp on stability of circuit.I have simulated the circuit using LTSP...

0693W00000HnvA4QAJ.png
SKuma.34 by Associate
  • 1041 Views
  • 0 replies
  • 0 kudos

Resolved! TDA7575B PCB Design

Hello there, I am newbie to PCB design and I am going to use TDA7575B. Here I have an input from a mobile which have two wires. I have few question regarding its design:Can I joint In1+ to In2+, In1- to In2- ? then those joints will be connected to s...

IHus.1 by Associate II
  • 2467 Views
  • 4 replies
  • 1 kudos