2023-05-25 5:14 AM
Hi,
during development I work with the CubeIDE and use JLink, it connects to the SWD-port of my STM-board properly and works like a charm within the IDE.
Now we're about to program loads of different boards. From my understanding this is where the CubeProgrammer shoukd be used. But when starting it, the JLink is not recognised, it only tells me about some ST-Link which could not be found (which is correct as it does not exist).
So how/where do I have to configure the CubeProgrammer to work with the JLink?
Thanks!
Solved! Go to Solution.
2023-05-25 11:44 AM
Unlike CubeIDE, the CubeProgrammer does not work with J-Link. But you can use the Segger J-Flash software for the same price.
2023-05-25 11:44 AM
Unlike CubeIDE, the CubeProgrammer does not work with J-Link. But you can use the Segger J-Flash software for the same price.
2024-05-23 3:18 AM
2024-10-14 6:11 PM
I just connected to a target using CubeMXProgrammer v2.17.0 connected via a J-Link.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.