2023-04-12 7:15 PM
We want to allow customers to download firmware directly.
Are you trying to pass the STM32CubeProgrammer\bin file, no licensing issues?
I'm trying to make a batch file so that I can download it right away.
I've tested it. If you pass only this file and the database file together, there seems to be no problem with downloading.
We ask if there will be any licensing issues if we pass this file on.
Solved! Go to Solution.
2023-04-26 12:31 AM
Hello @mkim.2 ,
Thanks for your feedback,
Yes, STM32CubeProgrammer can be redistributed and the license which must be used in this case is SLA0048.
I hope this helps,
Sara.
2023-04-26 12:31 AM
Hello @mkim.2 ,
Thanks for your feedback,
Yes, STM32CubeProgrammer can be redistributed and the license which must be used in this case is SLA0048.
I hope this helps,
Sara.
2023-05-01 1:10 AM
Hi,
We're also looking to do the same are. would you mind sharing how you plan to do this? are you jsut placing the cli.exe and licence and hex file in a folder to issue ?
2023-05-01 5:56 PM
thank you
Helped me a lot.
2023-05-01 5:58 PM
STM32_CLI
->Data_Base
->STM32_Programmer_CLI
-> libgcc_s_seh-1.dll
-> libstdc++-6.dll
-> libwinpthread-1.dll
-> Qt5Core.dll
-> Qt5Script.dll
-> Qt5SerialPort.dll
-> Qt5Xml.dll
-> STM32_Programmer_CLI.exe
2023-05-01 6:49 PM
We created a batch file and proceeded.
The CLI file worked well only when the above files were present.
"(CLI.exe Program Location)\STM32_Programmer_CLI.exe" -c port=COM5 br=115200 P=EVEN db=8 sb=1 -w "(hex file location).hex"
2023-05-01 9:14 PM
Fantastic, thanks for this
2023-05-01 9:29 PM
Thanks, what would be great, is if ST released the cubeprogrammer as uncompiled visual studio files so we could simply build our own GUI loaders
cheers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.