2021-09-25 1:08 AM
I can't flash to STM32 MCUs any more. after I accidentally wrote to Option bytes in STM32 CubeProgramming.
Now status is
PS C:\palm\programe\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin> .\STM32_Programmer_CLI.exe -c port=swd -ob displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-LINK SN : 066BFF525649898367213942
ST-LINK FW : V2J37M26
Board : NUCLEO-L432KC
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x435
Revision ID : Rev Z
Device name : STM32L43xxx/STM32L44xxx
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0x__
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 20 Bytes
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�? 100%�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0, reset level threshold is around 1.7 V)
User Configuration:
nRST_STOP : 0x1 (No reset generated when entering Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering Standby mode)
nRST_SHDW : 0x1 (No reset generated when entering the Shutdown mode)
IWDG_SW : 0x0 (Hardware independant watchdog)
IWDG_STOP : 0x0 (Freeze IWDG counter in stop mode)
IWDG_STDBY : 0x0 (Freeze IWDG counter in standby mode)
WWDG_SW : 0x0 (Hardware window watchdog)
nBOOT1 : 0x1 (Boot from system memory when BOOT0=1)
SRAM2_PE : 0x1 (SRAM2 parity check disable)
SRAM2_RST : 0x1 (SRAM2 is not erased when a system reset occurs)
nSWBOOT0 : 0x1 (BOOT0 taken from PH3/BOOT0 pin)
nBOOT0 : 0x1 (BOOT0 = 0, boot from system memory when nSWBOOT0=1 and main flash is empty,otherwise, boot from main flash memory)
PCROP Protection:
PCROP1_STRT : 0xFFFF (0x807FFF8)
PCROP1_END : 0x0 (0x8000000)
PCROP_RDP : 0x1 (PCROP zone is erased when RDP is decreased)
Write Protection:
WRP1A_STRT : 0xFF (0x807F800)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0xFF (0x807F800)
WRP1B_END : 0x0 (0x8000000)
How do I do?
2021-09-25 1:58 AM
Change connection to under reset and set write protection back or RDP back to 0. Simpler is use GUI utility as CLI.
2021-09-25 2:13 AM
Thank you for fast answer.
I will use GUI. I choose Mode: under reset connection. and Where I setting set write protection back or RDP back to 0?
2021-09-25 2:17 AM
I use for this old stlink utility, has menu option bytes. With new "Programmer" i dont help you.
2021-09-25 5:30 AM
Why can't you flash anymore? I don't see any errors in the log you posted.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.