2024-06-28 4:57 AM
Hello,
I have installed STM32CubeProgrammer (version 2.14.0) on a Linux machine. I have connected my NUCLEO-U575ZI-Q microcontroller to the machine, but the CubeProgrammer does not detect it (the machine does). I received this message on the CubeProgrammer:
ST-LINK error (DEV_CONNECT_ERR)
I tried the same setup on a Windows PC and it worked perfectly (with the same version of CubeProgrammer).
What could be the possible solution?
Best regards,
Solved! Go to Solution.
2024-06-28 5:49 AM
Could be an permission issue.
The required udev rules are in /etc/udev/rules.d directory?
Normally they must be installed manually. They can be found under the install path form STM32CubeProgrammer Drivers/rules.
2024-06-28 5:49 AM
Could be an permission issue.
The required udev rules are in /etc/udev/rules.d directory?
Normally they must be installed manually. They can be found under the install path form STM32CubeProgrammer Drivers/rules.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.