2018-11-20 7:19 AM
Hello,
after some fiddling, I can run STM32CubeProgrammer and I can see/update/connect to the stlinkv2 on nucleo boards. On the same machine, I can also connect to a STLINKV3 when running STM32CubeProgrammer/windows in a virtual box. However STM32CubeProgrammer/Linux and STLinkUpgrade/Linux can not see the StlinkV3.
Do I miss something? Is that known behaviour?
2018-11-20 11:15 AM
On my linux system, V3 connected to USB 2.0 port is detected by STLinkUpgrade and update mode can be activated. STM32CubeProgrammer detects V3, too. Don't have a target connected right now, so I can't confirm whether it actually works. (On USB 3.0 port, it is not detected.)
Maybe the udev rules are missing on your system? From my setup:
# stlink-v3 boards (standalone and embedded) in usbloader mode and standard (debug) mode
SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="374d", \
MODE:="0664", GROUP:="trusted", SYMLINK+="stlinkv3loader_%n"
SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="374e", \
MODE:="0664", GROUP:="trusted", SYMLINK+="stlinkv3_%n"
SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="374f", \
MODE:="0664", GROUP:="trusted", SYMLINK+="stlinkv3_%n"
2018-11-21 3:41 AM
I tested on a USB3 port. Testing on a USB2 hub connected to an USB3 Hub, the device is still not detected.
2018-11-21 4:08 AM
Same for me, USB-2.0 hub on USB-3.0 port: STLink V3 not detected. Only native USB-2.0 works.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.