2022-03-30 1:06 AM
Is it planned that in the future the cube programmer will also work with the j-link like the cubeIDE?
2022-03-30 7:20 AM
+1
We have one board that cannot work with ST-LINK because of design defect (to be fixed later);
It works with J-LINK in JTAG mode.
CubeIDE can use J-LINK for loading and debugging the program but I really miss full CubeProgrammer functionality - option bytes etc, that is hard with J-LINK software.
2022-04-12 2:59 AM
Hi @DS.5chäfer ,@Pavel A.
I see your point and will bring it up to the STM32CubeProgrammer team but to be honest it won't be treated in short term.
Internal ticket number: 126303 (PS: This is an internal tracking number and is not accessible or usable by customers).
Houda
2023-03-24 10:05 AM
Oh my gosh! I'd LOVE to use my J-Trace Pro with the STM32CubeProgrammer software.
2024-04-16 6:33 AM
Hi Pavel,
Can you please look into the following link. STM32CubeProgrammer & STM32CubeMonitor support SEGGER's J-Links
And please let me know which version of the cube programmer.
kind regards,
Abdul
2024-04-16 7:07 AM
V2.16.0 can do, see:
Which cube programmer version support jlink - STMicroelectronics Community
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.