2020-04-24 3:24 PM
I am using CubProgrammer (version 2.4.0) to update the flash on NUCLEO-G070 board.
When I select the device target i/f as ST-Link and connect, I can do flash programming.
When I select the target i/f is UART, the Com Port shows up correctly about this device. However, I couldn’t connect. The error message is:
Serial Port COM4 is successfully opened.
17:48:09 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
17:48:10 : Timeout error occured while waiting for acknowledgement.
17:48:10 : Timeout error occured while waiting for acknowledgement.
Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
Do I need to put the STM32G07 Boot0 pin LOW? What am I missing?
Another question:
Is the Flasher-STM32 a subset of the CubProgrammer? It can only do flash programming with target device i/f is UART?
2022-05-23 2:12 PM
Thanks dear,
I was frustrated for last 4 days as was not able to programme but your this small instruction solved my problem- Thanks a lot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.