STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

programming flash bank 2 sometimes fails with cli

I am using STM32CubeProgrammer (2.14.0) on Linux/Ubuntu 22.04 with NUCLEO-H563ZI.I do not observe any problem when I use the GUI application but I would like to use the CLI.I do not observe any issue when I write/download a program (elf or bin) to ba...

mete by Senior II
  • 1898 Views
  • 2 replies
  • 0 kudos

Resolved! STM32Cube Programmer Version 2.13.0

Dear ST Community, I would like to address an issue we have encountered while flashing the program on the STM32L562VETb microcontroller using different versions of the STM32 CubeProgrammer software. Our observations indicate a significant performance...

Kavan by Associate II
  • 5693 Views
  • 5 replies
  • 0 kudos

STM32Cubeprogrammer fails to install in MacOS

When starting install as described in documents, the setup icon appears and disappears directly. I tried to open the installer from the command line and then the following error message appears "LSOpenURLsWithRole() failed with error -10810 for the f...

JVers.6 by Associate
  • 6424 Views
  • 9 replies
  • 3 kudos

STM32CubeProgrammer (STM32CubeProg)

I just got the STM32F429I and cannot install STM32CubeProgrammer (STM32CubeProg) on my Mac running Ventura. Any guidance would be appreciated.It is quite sad and I can't return the devie to get a refund.

anietie by Associate
  • 1950 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.