STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32H753I-Eval2 in DFU mode

Hello,I'm curious if I am going through the correct procedure to put th H753I eval board in DFU mode. I have the power jumper JP10 on PSU. I then put a jumper on JP3 which is labeled BL_BOOT0 (which as far as I know puts the H7 in DFU mode when pulle...

TLuke.2 by Associate II
  • 9882 Views
  • 11 replies
  • 2 kudos

STM32H743 External loader problem

Hello,I'm learning STM32 and wrote an quadspi external loader for my NUCLEO -144 (STM32743ZI) and 1M external flash. I've it tested in the Cube IDE and everything looks OK, I can read and write the external flash. When I use the loader in STM32Cude...

YGU.1 by Associate II
  • 21129 Views
  • 19 replies
  • 0 kudos

Firmware Update

We have implemented a custom tool, which transfers a hex firmware file via USB DFU protocol to the control. While testing we had several problems sending the firmware to the control.First we extract the memory model out of the descriptor infromations...

Tedico by Associate II
  • 7372 Views
  • 2 replies
  • 1 kudos

Resolved! ST-LINK,Programmer error:DEV_TARGET_CMD_ERR

helloI used ST link to connect to stm32H743 and reported an error during the Programmer download process:"Error:ST-LINK error(DEV_TARGET_CMD_ERR)“.But,I used j-link to connect to stm32H743 and there were no errors during the stm32IDE download process...

jack-uni by Associate
  • 5385 Views
  • 3 replies
  • 2 kudos

Store data in internal flash using stm32g0x

Hi Team,I am using stm32g0x mcu to store the default chunk of data in to internal specific location for our data storage. Once it reboot it should read the default data.I tried with different mcu calls which will not synchronize with our platform.Ple...

Akuma.6 by Associate III
  • 1913 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeProgrammer Failure

Hello,The latest STM32CubeProgrammer (V 2.15.0) appears to be unable to program an STM32L471 microcontroller.It communicates successfully but fails with error:    Error: Operation exceeds memory limits    Error: failed to erase memoryThe hex file mem...

STM32 Cube PRG Fail.PNG
Chris21 by Senior III
  • 4185 Views
  • 3 replies
  • 3 kudos

No STM32 target found

Hi, I have been recently trying to leave my shallow nucleo side of the pool behind and swim towards the deeper end of the pool. But I feel like I'm drowning a bit and could use a lifeline... (:I have so far managed to connect to and write to, a small...

EOBD_1-1707333154936.png EOBD_2-1707334689895.jpeg
EOBD by Associate II
  • 4448 Views
  • 6 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.