STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Unable to connect microcontroller via stlink

Since configuring the STM32WB55CGU6 in STM32Programmer with the following settings, I am no longer able to connect to the chip using ST-Link. I cannot download programs in Keil, and the ST-Link in STM32Programmer cannot connect either. Changing the p...

ST-LINK V2 does not work

Hi!I would like to ask for a little help. I have a LoraWan E5 wich I want to program with ST-Link V2, but as soon as I want to connect to it in the STM32CubeProgrammer I get the errors below. I also attached the pinout that I follow. I connect SWDIO,...

JSON output for STM32_Programmer_CLI.exe

Hi!I wanted to ask the following: Is it possible to get the output of STM32_Programmer_CLI.exe as JSON?We use the CLI within one of our internal software tools and the parsing of the output is a little brittle. A structured output format would help a...

Resolved! STM32CubeProgrammer V2.16 DFU Download Problem

Hi,Updated from 2.15 today. Having DFU download problem seen attached.Board is recognised but upper right still stated as "Not connected" and download fails.Downgraded to V2.15 and same board connects and downloads OK. OS: W10 64bitBoard: STM32F767NI...

TKana.1 by Associate III
  • 7898 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.