STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

I used STM32CubeProgrammer v2.1.0 in utuntu 18.04. Connect STM32F103ZET6 failed. Usb to serial port is WCH CH340G.

13:05:04 : Serial Port ttyUSB0 is successfully opened.13:05:04 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off13:05:05 : Timeout error occured while waiting for acknowledgement.13:05:05 : Timeo...

ljing.17 by Associate
  • 873 Views
  • 0 replies
  • 0 kudos

Cannnot start STM32CubeProgrammer.app

I just installed STM32CubeProgrammer on my Mac running MacOS Mojave with Java 8 installed. Everything installs OK. But I cannot run the app. I have tried Show Contents on the .app file and run /Applications/STMicroelectronics/STM32Cube/STM32CubePr...

spdaly by Associate II
  • 731 Views
  • 0 replies
  • 0 kudos

I'm trying to program a stm32l031k6 MCU using the UART interface and cube programmer.

BOOT0 is high and the chip is reset. Using the following command:./STM32_Programmer_CLI -c port=/dev/ttyUSB0 -vb 3 -ob displi'm getting the following result:     -------------------------------------------------------------------                     ...

Fabry by Associate
  • 1686 Views
  • 2 replies
  • 0 kudos

STM32 Cube Programmer API

Besides function "downloadFile", is there a way of program flash using a buffer ?The use case is not to have a firmware file, protecting the programming phase on third parties (assembly lines, testing).

rbenv.3 by Associate II
  • 1403 Views
  • 2 replies
  • 0 kudos

How can I program STM32L011 prototype board

Hello all,I am using STM32L011K6_Nucleo Board for developing a smart application, now I making prototype with STM32L011 microcontroller and some other sensors. My doubt how should I program my prototype board? what are the connection do I have to lea...

VDhan by Associate II
  • 2341 Views
  • 3 replies
  • 0 kudos

Resolved! Unable to Run STM32CubeProgrammer

Hi, I have installed STM32CubeProgrammer but unable to run it. I get the message:"CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java architecture"I see other have had this and upgrading to...

MWill.18 by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

Download firmware to STM32F4 in PCB assembly line

This week I am about to start production of my embedded product using STM32F411. I need a simple way to drag n drop firmware.ELF into a batch or exe that downloads and verifies. I am digging into the STM32CubeProgrammer documentation, but I have not ...

AColl by Associate
  • 1999 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to flash new firmware on STM32L031C6

I have been flashing ST with the Flash Loader Demo utility successfully for long time, directly to my PCB design. BOOT0 pin is high, everything around the STM32 is quite (no activity on peripherals connected). Reset properly connected to a Resistor w...

javqui by Associate II
  • 2869 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.