STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! [SOLVED] Problem running STM32CubeProgrammer

When running the program STM32CubeProgrammer, an error message appears, saying:"CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java architecture". However I have the lastest JAVA SE Run Tim...

protect sector when upload in dfu

Hi,I started developing a project for stm32l072cz. After seeing dfu mode working correctly I realized a problem. The objects that I program through the j-link Segger are serialized and when I go to upload the dfu file, the serialization is deleted. I...

Error: Data mismatch found at address 0x08001504 (byte = 0xF7 instead of 0x7B) Error: Download verification failed

I've connected an STM32F407-G-DISC1 board to debug a DIY-MORE breakout board. The debuggee is connected via SWDCLK,SWDIO, NRST to the STLINK-SWD interface of the DISC1 board. Discovery jumpers are off, ST-LINK enabled.I'm loading a blinky app but whe...

STM32CubeProgrammer graphical Windows working, same hardware STM32CubeProgrammer Cmd Line is not working,

CubeProgrammer under Windows (graphical Version) is working fine. CubeProgrammer with Cmd Line brings error:Output     -------------------------------------------------------------------                     STM32CubeProgrammer v2.10.0    ------------...

0693W00000KdYTeQAN.jpg 0693W00000KdYUDQA3.jpg
franz2 by Associate III
  • 1965 Views
  • 1 replies
  • 0 kudos

ST32F413 Won't Program in Cube Programmer?

I have two identical pre-production PCBs containing fresh, unprogrammed 32F413VGT micros from our distributor. One board will program just fine but CubeProgrammer says "can't erase device!" when I try to program the other board.After first scanning ...

JOlso.12 by Associate III
  • 1438 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0 unable to connect via SWD

I tried to connect the STLink to the STM32G030K6T6 by connecting SWCLK SWDIO VDD and GND pins, but the STM32CubeProgrammer can't detect the MCU.I also tried to check with the logic analizer the pins and there is only a little signal from the stlink b...

FMill.2 by Associate
  • 2857 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.