STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

How to change scaling or font size on Linux

Hi, StM32CubeProgrammer shows up realy tiny on my Linux laptop screen (2560:1600), please see screenshot.Something similar happened to STM32CubeMx inside the IDE, I could fix that starting the IDE withGDK_DPI_SCALE=0.5 GDK_SCALE=2 /opt/st/stm32cubeid...

0693W00000D2UZCQA3.png
CDenk.1 by Associate II
  • 4996 Views
  • 4 replies
  • 1 kudos

How internal flash of STMU575/585 can be protected from copying during firmware update at manufacturer/customer side?

We deliver encrypted image to the customer-manufacturer. After image update is performed the image is stored opened in internal flash. With RDP level set to 2 it is possible protect from jtag debugging and access. But if hacker at manufacturer side, ...

VTver.1 by Associate III
  • 2623 Views
  • 4 replies
  • 0 kudos

Unable to read device id from ROM table

Hi everyone,I have a st-link v2 with the STM32cube programmer on a windows 10 PC. My target is a ISP30301 ( nrf 518222) . If i try to connect to the target , it says "Unable to read device id from ROM table". (after the hardware reset is done) . What...

fpatr.1 by Associate
  • 5996 Views
  • 9 replies
  • 0 kudos

Resolved! STM32CubeProgrammer doesn't show DBANK option byte

Hi !I'm using STM32CubeProgrammer v2.12.0 (according to the updater it is the latest at this time) and I want to enable Dualbank on my Nucleo board.The Nucleo board is a NUCLEO-L476RG and is correctly recognized as such: However in the Option bytes -...

_legacyfs_online_stmicro_images_0693W00000bhiDwQAI.png _legacyfs_online_stmicro_images_0693W00000bhiELQAY.png
SDpy.1 by Associate II
  • 3490 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.