2022-05-11 12:45 PM
What's the difference between "aci_gatt_update_char_value" and "aci_gatt_write_char_value"?
In addition, what is "aci_gatt_write_without_resp"?
Is it faster than others to send data?
How can I active "aci_gatt_write_without_resp"?, because it is inactive in STM32cubeMX during the BLE setup.
2022-05-13 10:51 AM
I'm reading PM0271 and I found the answer.
The update is used when the Server notifies a value to the client.
The read/write is used when the client wants to interact with the server.
Am I right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.