2020-10-07 10:17 PM
Hello,
I had both the ProjectManager.TemplateDestinationPath and ProjectManager.TemplateSourcePath pointing to folder which did not exist.
So, I updated `ProjectManager.TemplateSourcePath` to
`ProjectManager.TemplateSourcePath=C\:\\STM32CubeMX\\db\\extra_templates` as the STM32CubeMX folder is present in C Drive in the ROOT C directory.
What is the use of `ProjectManager.TemplateDestinationPath`? I am not sure what should be the value passed to `ProjectManager.TemplateDestinationPath`. For now I have assigned the path where the IOC file containing these settings exist:
`ProjectManager.TemplateDestinationPath=E\:\\DEPT197\\GIT\\Gateway-H7-All-Codes\\Gateway-H7\\Gateway-H7-App`
Can I safely remove these two settings / variables, as others might have a different setup / folder for STM32CubeMX, templates, etc.
Please suggest.
Thanks and regards,
Rajeev
Solved! Go to Solution.
2020-10-12 3:15 AM
Hello @Rajeev Arora
Where did you faced this issue ?
The Default Template Settings Source Folder location should be " C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\db\extra_templates" and the Default Template Settings Destination Folder should take your "Project Location".
Regards,
Khouloud
2020-10-12 3:15 AM
Hello @Rajeev Arora
Where did you faced this issue ?
The Default Template Settings Source Folder location should be " C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\db\extra_templates" and the Default Template Settings Destination Folder should take your "Project Location".
Regards,
Khouloud
2020-12-07 6:42 AM
Dear @Khouloud ZEMMELI ,
Thanks for the update, I probably missed reading your inputs, and hence replying today.
I had been using the STM32CubeMX version 5 and later STM32CubeMX version 6 for creating the IOC files and later migrating them to newer version as and when the STM32CubeMX newer version gets available.
I've been observing some of my IOC files (when viewed using NOTEPAD++) have the two variables, whiles others do not have it.
Attached image contains the folder structure available on C:\
I had to create separate folder for Software and another folder for Packages, so that:
Thanks,
Rajeev
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.