2022-11-29 2:48 AM
Today my STM32CubeIDE does an update to the Version: 1.11.0 (Build: 13638_20221122_1308 (UTC) ) including the CubeMX Version: 6.7.0-RC2 (Build: 20221118-1646 (UTC))
Using the FreeRTOS Middleware the generation of the main file has a big bug. There will be the "USER CODE Header" lines instead of the FreeRTOS lines inseide the main()-function.
This happens also if I create a new empty project using the FreeRTOS middleware. It will generate the attached main-c-file. See lines 145-151.
I haven't searched where the bug comes from.
2022-11-30 4:37 AM
Having the same problem after updating STM32CubeIDE. I think this is a bug in STM32CubeMX made by ST developers.
2022-11-30 8:24 AM
I have tested a little bit with manual editing the ioc-file.
this were the lines before updating STM32CubeIDE:
MxCube.Version=6.6.1
MxDb.Version=DB.6.0.60After the update this changed to:
MxCube.Version=6.7.0
MxDb.Version=DB.6.0.70The code generation worked in correct way if I change to:
MxCube.Version=6.7.0
MxDb.Version=DB.6.0.61but it does the same stupid thing if I use the new database:
MxCube.Version=6.6.1
MxDb.Version=DB.6.0.70So it seams a problem inside the database
2022-11-30 8:59 AM
I have found it :grinning_face:
Inside the FREERTOS-STM32F4xx_Configs.xml file is a error in line 349
line 349: <RefConfigFile Description="Variable creation then launch the RTOS" Name="CREATION_V2" Template="?freertos_init_c_cmsis_v2.ftl">
line 350: <File Category="source" Condition="all" Name="rtos_obj_creat.tmp" Version="10.3.1"/>
<Argument Comment="User threads" GenericType="rtos_list" Name="Threads"/>
<Argument Comment="User queues" GenericType="rtos_list" Name="Queues"/>
<Argument Comment="User timers" GenericType="rtos_list" Name="Timers"/>
<Argument Comment="User mutexes" GenericType="rtos_list" Name="Mutexes"/>
<Argument Comment="User recursive mutexes" GenericType="rtos_list" Name="RecursiveMutexes"/>
<Argument Comment="User binary semaphores" GenericType="rtos_list" Name="BinarySemaphores"/>
<Argument Comment="User counting semaphores" GenericType="rtos_list" Name="Semaphores"/>
<Argument Comment="User events" GenericType="rtos_list" Name="Events"/> <!-- NEW FOR EVENTS -->
<Argument Comment="API in use" GenericType="simple" Name="FreeRTOS_API"/> <!-- need to distinguish CMSIS v1 and v2 -->
</RefConfigFile>There is a question mark as first sign of the template name. Remove it and it works.
I have done a short view on other FREERTOS-STM32F configs. They are without this error.
This files comes with the STM32CubeIDE-update. So it will be overwritten if it does a new (re-)update
2022-11-30 9:04 AM
Do you work with an STM32F4xx controller? I have solved the problem :)
2022-11-30 11:45 AM
Indeed, the problem was in this sign "?" in FREERTOS-STM32F4xx_Configs.xml ....Probably someone joked in ST :face_with_tears_of_joy:. Now appeared an initialization of tasks, semaphores, mutexes after calling the osKernelInitialize() function. Thanks buddy!
2022-12-01 7:41 AM
Hello @Jens Räthe
Thank you for your contributions and for your detailed explanations,
I confirm the issue on my side, it has been reported to STM32CubeMX development team .
Internal ticket number: 140318(This is an internal tracking number and is not accessible or usable by customers).
I will keep you posted with updates.
Regards,
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-22 10:33 PM
It's been 3 months and a newer version of STM32CubeMX has been released, but the problem still hasn't been solved.
2023-03-07 1:15 AM
Hello @Jens Räthe
I am glad to inform you that the Internal ticket number: 140318 is fixed and integrated in the latest CubeMX version 6.8.0 .
This is the LINK for downloading it .
Thanks again for your contributions .
Ghofrane
Ghofrane.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.