2020-12-22 11:43 AM
Code generated by CubeMX
static void MX_SDMMC1_SD_Init(void)
{
/* USER CODE BEGIN SDMMC1_Init 0 */
/* USER CODE END SDMMC1_Init 0 */
/* USER CODE BEGIN SDMMC1_Init 1 */
/* USER CODE END SDMMC1_Init 1 */
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockBypass = SDMMC_CLOCK_BYPASS_DISABLE;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 0;
HAL_SD_Init(&hsd1);
/* USER CODE BEGIN SDMMC1_Init 2 */
BSP_SD_Init();
HAL_Delay(200);
/* USER CODE END SDMMC1_Init 2 */
}There is a function in - SDMMC_GetCmdResp1(SD MMC x, SD MMC_CMD_UP_CMD, SD MMC_CMD TIMEOUT);
When the Sdmmc->STA register is checked in the body of this function, the check takes a very long time, since the CMDACT bit is in one. After 20-30 seconds, the bit is reset and the card works perfectly. Tellingly, the initialization time may be shorter, sometimes everything passes at once.
4-bit mode, 48 MHz frequency.
How to fix?
2020-12-23 12:56 PM
P.s. I tested with a debugger that where fail the program. Inside of the SD_PowerON function exist a while loop. When the cards don't recognize this while loop run infinitelly and never go out from there.
/* Send ACMD41 SD_APP_OP_COND with Argument 0x80100000 */
while(validvoltage == 0)
{
if(count++ == SDMMC_MAX_VOLT_TRIAL)
{
return HAL_SD_ERROR_INVALID_VOLTRANGE;
}
/* SEND CMD55 APP_CMD with RCA as 0 */
errorstate = SDMMC_CmdAppCommand(hsd->Instance, 0);
if(errorstate != HAL_SD_ERROR_NONE)
{
return HAL_SD_ERROR_UNSUPPORTED_FEATURE;
}
/* Send CMD41 */
errorstate = SDMMC_CmdAppOperCommand(hsd->Instance, SDMMC_STD_CAPACITY);
if(errorstate != HAL_SD_ERROR_NONE)
{
return HAL_SD_ERROR_UNSUPPORTED_FEATURE;
}
/* Get command response */
response = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP1);
/* Get operating voltage*/
validvoltage = (((response >> 31) == 1) ? 1 : 0);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.