cancel
Showing results for 
Search instead for 
Did you mean: 

User LED2 mapping bug on Nucleo-H753ZI

KishoreK31
Associate

Hello, 

 

Began learning STM32 MCUs with my Nucleo-H753ZI board and I think I found a bug. 

The IO configurator on CubeIDE thinks user LED2 is on PB7 and is blue coloured. I'll paste the code it generates below. But in fact, the user manual UM2407 says user LED2 is on PE1 and is yellow coloured, which is indeed correct. 

Generated code from CubeIDE for Nucleo-H753ZI:

#define LED2_PIN                                GPIO_PIN_7
#define LED2_GPIO_PORT                          GPIOB

 Appears to be a bug that should be fixed in the BSP.

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @KishoreK31 and welcome to the ST community,

It will be escalated internally for analysis and an eventual analysis. Internal Ticket 218959 has been submitted which is not accessible by the community users.

Thank you for your contribution.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello @KishoreK31 and welcome to the ST community,

It will be escalated internally for analysis and an eventual analysis. Internal Ticket 218959 has been submitted which is not accessible by the community users.

Thank you for your contribution.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
eodudrepublic
Associate

### In `stm32h7xx_nucleo.h` :

/** @defgroup STM32H7XX_NUCLEO_LOW_LEVEL_Exported_Types LOW LEVEL Exported Types
  * @{
  */
#if defined (USE_NUCLEO_H745ZI_Q) || defined (USE_NUCLEO_H755ZI_Q) || defined (USE_NUCLEO_H743ZI2) ||\
    defined (USE_NUCLEO_H7A3ZI_Q) || defined (USE_NUCLEO_H723ZG)
typedef enum
{
  LED1 = 0,
  LED_GREEN = LED1,
  LED2 = 1,
  LED_YELLOW = LED2,
  LED3 = 2,
  LED_RED = LED3,
  LEDn
}Led_TypeDef;
#else /* USE_NUCLEO_H743ZI || USE_NUCLEO_H753ZI */
typedef enum
{
  LED1 = 0,
  LED_GREEN = LED1,
  LED2 = 1,
  LED_BLUE = LED2,
  LED3 = 2,
  LED_RED = LED3,
  LEDn
}Led_TypeDef;
#endif

There are no "NUCLEO_H753ZI", maybe that's the reason.

The OP is not using the BSP driver for this board but rather the CubeMx configuration that configures the pins by default for this board.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.