2024-06-01 1:27 AM
im trying to interface STM32H743ZI with FT2232 USB MINI MODULE .
1--> anybody did this type of task ,please share me the link of your project .(especially i need to know names of the pins to be connected each between ) .
2--> i found some similar pins in my board and mini module .. but i didnt find 3 pins in FT2232 which are available in my board. that pins are 1 . DIR , 2. STP , 3. NXT. so if anybody knows about it please let me know the pin names to be connect with the FT2232 (above 3 pins with FT2232) .
2024-06-01 2:14 AM
FT2232 USB MINI MODULE
WHAT module you talk about ?
show pic, link, pdf .
2024-06-01 2:52 AM
2024-06-01 2:55 AM
2024-06-01 3:17 AM
Ok,
and STM32H743ZI is ... custom ? or ?
+
Why you want connect a "multi-usb-interface" to a H743 , that has two (!) USB interface on chip ??
2024-06-01 3:48 AM
i just trying to check with the stm32 on chip USB_OTG_HS to mini module and mini module to another external device which can give me the packets continuously . so i will receive the packets from external device to my mini module and i ll send that packets to my stm32h7controller .
so here i need to know the exact pins to connect my controller to mini module
2024-06-01 4:50 AM
Well, i cannot find my big blue crystal ball, so...
whats "my controller" ? which signals/lines you have/connect and send ?
What should it do then ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.