cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H725ZGT6 custom board hangs (Cube, Keil, ULINK2)

TimK1
Associate II

Hello,

 

i am using the STM32H725ZGT6 on a custom layout.

As comparison i am also using the STM32H723ZGT6U on a NUCLEO-H723ZG Board.

I am using STM32CubeMX, Keil µVision and the ULINK2 debugger. 

 

To test the Serial Wire Flashing procedure, i created an empty Cube Projext (using HSI and no controller pins), compiled itand flashed it to the controller. The Nucleo Board works perfectly fine with this setup.

 

However when i do the exact same procedure (of corse with correct controller), my custom Board has a problem:

I can only flash the software when the BOOT0-Pin is set to +3V3 (but not use any peripherals). When the BOOT0-pin is set to GND, i cannot program anymore and there is "SWD Communication Failure" according to Keil. I also tried to toggle a GPIO but had no acces with my custom board so far.

Any ideas on this?

If you need more infos, please let me know.

See Layout files attached. Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Check LDO vs SMPS settings in your System Clock Configuration code.

Check VOS and PLL settings.

Check HSE_VALUE 

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4
Imen.D
ST Employee

Hello @TimK1 

Is GND connected to the debugger? Try powering the board directly from the debugger.

Check the debugger settings to set correct debugger and use SWD.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Check LDO vs SMPS settings in your System Clock Configuration code.

Check VOS and PLL settings.

Check HSE_VALUE 

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hello Imen,

thank you for the reply. Yes, i have connected GND and VCC to my custom board. However i think the ULINK2 is not able to power the board. It has a jumper +3V3 / VCC / ARM. But this only powers the SWD signals, not the VCC of the board (as far as i can see). I tried both jumper positions with no change of the outcome. 

Greets, Tim

Hello Tesla,

thanks for your reply. This solved my problem. 

In STM Cube i had the wrong setting. (SMPS instead of LDO):

System Core -> RCC -> Parameter Settings -> Power Parameters -> PWR_LDO_SUPPLY

Thank you very much!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.