2020-03-17 3:34 AM
Hi,
I want to connect USB Mouse with my Discovery Board and want to communicate with USB protocol. Where
USB device --->> USB mouse
USB HOST --->> STM32F407VGT6 Discovery Board.
IDE --->> STMCube IDE and STMCubeMX for HAL Library for easy understanding.
Questions :
Q.1: I am not getting any example so i can test. I am sure Mouse and Keyboard examples are very common but I am not getting easily.
Q.2: I tried by myself using HAL library but When I am connecting my mouse with "Board". My mouse is not getting any power because Red Led which mouse has, is not glowing. Which directly means emuration process fails. Although I check my hardware which seems perfectly fine. except I am not getting 5V to operate a wired mouse.
I am attaching schematic for your reference where you can search CN5.
Can anyone face similar issue with this Board ?
Q.3: I used you Function which i add by myself into main file.
-->> USBH_StatusTypeDef USBH_HID_MouseInit(USBH_HandleTypeDef *phost);
-->> HID_MOUSE_Info_TypeDef *USBH_HID_GetMouseInfo(USBH_HandleTypeDef *phost);
Thanks & Regards
Vivek Yadav
2020-03-18 5:44 AM
Hi,
Let me update about my problems.
1: I found example code within HAL library by seeing STMicroelectronics youtube channel.
2: while searching I lost connection with on board debugger. Now it is not working. and I am using external debugger for programming my board.
But some how I am able to connect my wireless mouse with my Discovery board.
HOW I did this.
I make my VBUS pin which is PA9 in my case. I config this pin in output mode and make high so I get power supply of 3V and wireless mouse able to send its report. Where as wired mouse is still not working as expected because it requires 5V.
Now I am on my next task.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.