2015-04-02 6:00 PM
Hello
everyone,
I have trouble with getting ADC values over DMA.
I saw example :STM3210E_EVAL\Examples\ADC\ADC_Sequencer and create project in MXCube with 13-ADC channels after generate code and launch project I am got only ch0 value other values set as zero.
*Interrupt HAL_ADC_ConvCpltCallbackhas been occurred.
My initialization code:
void
MX_DMA_Init(
void
)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}
/* ADC1 init function */
void
MX_ADC1_Init(
void
)
{
ADC_ChannelConfTypeDef sConfig;
/**Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 13;
hadc1.Init.NbrOfDiscConversion = 13;
HAL_ADC_Init(&hadc1);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 2;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_3;
sConfig.Rank = 3;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_6;
sConfig.Rank = 4;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_7;
sConfig.Rank = 5;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = 6;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = 7;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = 8;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_11;
sConfig.Rank = 9;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_12;
sConfig.Rank = 10;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_13;
sConfig.Rank = 11;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_14;
sConfig.Rank = 12;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_15;
sConfig.Rank = 13;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
}
void
HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
RCC_PeriphCLKInitTypeDef PeriphClkInit;
GPIO_InitTypeDef GPIO_InitStruct;
if
(hadc->Instance==ADC1)
{
/* USER CODE BEGIN ADC1_MspInit 0 */
/* USER CODE END ADC1_MspInit 0 */
/* Peripheral clock enable */
__ADC1_CLK_ENABLE();
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADC;
PeriphClkInit.AdcClockSelection = RCC_ADCPCLK2_DIV6;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit);
/**ADC1 GPIO Configuration
PC0 ------> ADC1_IN10
PC1 ------> ADC1_IN11
PC2 ------> ADC1_IN12
PC3 ------> ADC1_IN13
PA0-WKUP ------> ADC1_IN0
PA1 ------> ADC1_IN1
PA3 ------> ADC1_IN3
PA6 ------> ADC1_IN6
PA7 ------> ADC1_IN7
PC4 ------> ADC1_IN14
PC5 ------> ADC1_IN15
PB0 ------> ADC1_IN8
PB1 ------> ADC1_IN9
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
|GPIO_PIN_4|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_3|GPIO_PIN_6
|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* Peripheral DMA init*/
hdma_adc1.Instance = DMA1_Channel1;
hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_adc1.Init.Mode = DMA_CIRCULAR;
hdma_adc1.Init.Priority = DMA_PRIORITY_VERY_HIGH;
HAL_DMA_DeInit(&hdma_adc1);
HAL_DMA_Init(&hdma_adc1);
__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
/* System interrupt init*/
HAL_NVIC_SetPriority(ADC1_2_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(ADC1_2_IRQn);
/* USER CODE BEGIN ADC1_MspInit 1 */
/* USER CODE END ADC1_MspInit 1 */
}
}
void
DMA1_Channel1_IRQHandler(
void
)
{
/* USER CODE BEGIN DMA1_Channel1_IRQn 0 */
/* USER CODE END DMA1_Channel1_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_adc1);
/* USER CODE BEGIN DMA1_Channel1_IRQn 1 */
/* USER CODE END DMA1_Channel1_IRQn 1 */
}
void
HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc){
}
void
HAL_ADC_ConvCpltCallback( ADC_HandleTypeDef * hadc){
xSemaphoreGiveFromISR(_dma_ready_sem, NULL);
}
Start:
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)table, 13);
//wait complete
//result:167, 0, 0, 0 ,0, 0, 0, 0 ,0, 0, 0, 0, 0
What else is required to run the ADC?
Or this problem in library?
Best Regards,
Krasutski Denis
#stm32f103-cubemx-dma-adc2015-04-02 10:56 PM
I has been try launch
ADC_Sequencer on my board.
I got some result after launch:if
(HAL_ADC_Start_DMA(&AdcHandle,
(uint32_t *)aADCxConvertedValues,
ADCCONVERTEDVALUES_BUFFER_SIZE
) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
aADCxConvertedValues contain only one values, other zero, dma interrupts not occurred!
But this array filled after run 3 times:HAL_ADC_Start(&AdcHandle);
/* Wait for conversion completion before conditional check hereafter */
HAL_ADC_PollForConversion(&AdcHandle, 1);
It is normally? for get all ADC values I shuld run
HAL_ADC_PollForConversion several times?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.