2018-04-11 4:31 AM
Dear Cube team,
Just noticed that STM32CubeMX v 4.24.0 does not show correct mode for GPIOs in pinout view (the main nice GUI).
On the picture below, PF14 is GPIO input with pullup, but the flyout tip shows as (no mode).
Would like to see the actual mode there.
Thanks,
-- pavel
#stm32f4 #cubemx-v4.24Solved! Go to Solution.
2018-04-12 8:10 AM
OK, I understand your request and will raise it to our STM32CubeMX team.
So it is a generic issue and not really related to a given board where the pinout view has to reflect the GPIO configurations.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-04-11 7:23 AM
Hi
pavel_a
,Could you please precise the board you are using?
Best way is to share your .ioc file.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-04-11 1:48 PM
Amel,
It is a custom board. The part is STM32F446. I've attached the .ioc.
Thanks,
PavelA
2018-04-12 8:10 AM
OK, I understand your request and will raise it to our STM32CubeMX team.
So it is a generic issue and not really related to a given board where the pinout view has to reflect the GPIO configurations.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-10-16 1:21 AM
Hello,
Please note that a fix was deployed in STM32CubeMX 5.4.0, already available on the web.
You can install this new version and check it.
More details about this release are provided on https://community.st.com/s/question/0D50X0000BTeOGVSQ3/stm32cubemx-540-released.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.