2019-04-11 6:37 PM
In some cases the USER sections are not sufficient to make some needed modifications to the HAL drivers. When modifying a configuration in STM32CubeMX, it would be useful to be able to flag drivers so that they are not overwritten when the code is generated.
Obviously, one can work around the current scheme by inserting code in the IRQ handler call, and include other routines with names that do not conflict with the HAL driver names, but that becomes a bit of a mess, especially when there is only minor change called for in the HAL driver.
2019-04-11 8:45 PM
Here we uniquely name the things we change in the HAL and keep local copies in the project directory
stm32h7xx_hal_sd_localized.c
It is a) obvious that a modified file is being used, b) it can be readily fixed again or ported into another project, c) falls within the scope of source management separate from the unmodified library code.
CubeMX often uses a "nuke it form orbit" approach because otherwise they'd get swallowed by support issues, from things like metastability and loops, where everytime you build you get something different.
2019-04-13 5:55 PM
One solution not involving CubeMX would be to save the HAL routines that are user modified in a directory. When CubeMX is run and the project code regenerated, with a trivial script, copy the saved files back in, overwriting the the regenerated routines. Of course updates to the original HAL routines are lost, but when one is groveling in the details of the driver one is off on a different course with the driver anyway.
Having done bare-metal on the STM32 for about five years, I find CubeMX, (in order of value)--
The actual drivers are ok for most ordinary applications, and good for those new to the product. However, the big time and effort savings is the above three items. In my experience, getting the pins and peripheral registers setup and initialized was a major part of the effort of using these processors and the CubeMX effort is on the right path.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.