2019-03-04 1:10 AM
This result in compilation error since dynamic allocation is disabled and only static is used.
For admins: If .ioc file needed, please write me a PM and I'll send it. This is something which I wouldn't want to put here as public.
Atollic console:
"Description Resource Path Location Type
'configTOTAL_HEAP_SIZE' undeclared here (not in a function) heap_2.c /IWWT_M2_Processing_Fw/Middlewares/Third_Party/FreeRTOS/Source/portable/MemMang line 67 C/C++ Problem
#error This file must not be used if configSUPPORT_DYNAMIC_ALLOCATION is 0 heap_2.c /IWWT_M2_Processing_Fw/Middlewares/Third_Party/FreeRTOS/Source/portable/MemMang line 50 C/C++ Problem
"
2019-03-04 8:28 AM
Hi. I ran into the same thing. I use SW4STM, and if you right-click on the heap_x.c file, and go to Resource Configuration->Exclude From Build, it survives future CubeMX ‘Generate Source Code’ activities. I hope this helps.
2019-03-04 8:37 AM
Yes, I know it. It might be handy for somebody, I forgot to mention it. But it's still a bug.
2019-10-03 12:23 AM
Any news please?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.