2024-07-11 5:31 PM
Could you please tell me relationship between maximum peripheral frequency on STM32 datasheet and actual clock config value in CubeMX?
As an example, I'm currently working with STM32H573RIT6.
The maximum USB clock in this MCU's datasheet (Table.22) is 50MHz.
However, when I actually enable USB in CubeMX and set clock, I can set it to same value as FCPU (250MHz) without getting an error.
The same phenomenon occurs for other peripherals whose maximum clock is less than the FCPU.
I was wondering about discrepancy between this datasheet and actual clock.
Also, many peripherals use HCLK/PCLK as default clock source, but HCLK/PCLK is basically same value as FCPU, so I would like to know why peripherals whose maximum clock is less than FCPU operate at default value.
Thank you.
2024-07-12 2:35 AM
Hello @dojyorin
Thank you for bringing this issue to our attention, I will check it internally and get back to you as soon as possible.
Thx
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.