2023-06-22 1:30 AM - edited 2023-06-22 2:46 AM
I have selected NUCLEO-L073RZ as per our development board specification.
Similarly, I am using the manufacturer specified version below.
I am using STM32CubeMX version 6.0.1.
The Firmware Package Name and Version is STM32Cube MCU Package for STM32L0 1.11.3.
Kail version is uVision V5.29.
When I opened the project in Keil and tried to compile the new, I got following error :
startup_stm32l073xx.s: error: A1023E: File "C:/Users/<user-name>/STM32Cube/Repository/STM32Cube_FW_L0_V1.11.0//Drivers/CMSIS/Device/ST/STM32L0xx/Source/Templates/arm/startup_stm32l073xx.s" could not be opened: No such file or directory
I just verified the directory
I found that the directory was empty, hence the project couldn't compile.
Hence, I have following questions:
Why does the 'C:\Users\<user-name>\STM32Cube\Repository\STM32Cube_FW_L0_V1.11.0\Drivers\CMSIS' show empty?
2023-06-22 2:16 AM
Hello,
Firstly, STM32CubeMX version 6.0.1 is quite old, maybe you want to migrate to 6.8.0.
Secondly, it is strange that your project is looking for the CMSIS files in C:/Users/<user-name>/STM32Cube/Repository/STM32Cube_FW_L0_V1.11.0
when you are using STM32Cube MCU Package for STM32L0 1.11.3
it should be C:/Users/<user-name>/STM32Cube/Repository/STM32Cube_FW_L0_V1.11.3
so maybe you want to check whether this path exists as well, and make your project take the files from there.
In any case, with the latest CubeMX 6.8.0 you can still download the V1.1.13 package again if you need.
Hope that helps.
Best regards
2023-06-22 5:41 PM - edited 2023-06-22 5:45 PM
Hi, Mike_ST
Thank you for your reply.
Attached files are the project manager screen.
The firmware package version is displayed so that we can select either 1.11.0 or 1.11.3, but selecting 1.11.3 will result in an error.
Could you give me some advice on how to deal with it?
Best regards,
sss_jpn
2023-06-29 4:56 PM
Hi, experts.
Can anyone give me advice on my problem?
Best regards
2023-06-30 6:21 AM
Hello,
Sorry for late answer,
With STM32CubeMX 6.8.0 (I can't test with 6.0.1, as it is too old)
Click "Help Menu"=>"Check for updates"
Click "Help Menu"=>"Updater settings" and remember the repository folder path
Click "Help Menu"=>"Manage embedded software packages"
Select STM32L0 package version 1.11.3
click "install"
It will download some files.
In the previous repository folder, check that you have the "stm32cube_fw_l0_v1113.zip"
file and the "STM32Cube_FW_L0_V1.11.3" directory.
in the CubeMX open "Project Manager" tab
Don't select "Use latest available version"
Don't select "Use default Firmware Location"
and in "Firmware Relative Path" browse for the location of the "STM32Cube_FW_L0_V1.11.3" directory
Please don't select STM32F0 firmware directory when you are using an STM32L0 product as I see that in one of your pictures.
Hope that helps,
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.