2019-03-19 3:39 AM
Hello,
Using STM32H753VITx with STM32CubeMX 5.1.0, I would like to use SAI1-A as 'Master with MCO' and external synchro out, and SAI4-A as synchronous slave.
SAI4-A doesn't show the synchronous slave option.
Alternatively I could do it the other way round, with SAI1-A slaving synchronously to SAI4, but that doesn't appear as an option either.
With the LQFP144 and LQFP176 packages I can select these options.
I don't believe there is a pinmux issue, as the SAI1/4 data pin is not used by any other SAI.
Is this just a problem with CubeMX or is there an underlying limitation of the LQFP100 package that is causing this?
Thanks and best regards,
Kieran.
2019-03-19 3:43 AM
Hello @graffiti
Your request is reported internally for further check.
Best Regards,
Khouloud
2019-03-19 8:06 AM
@graffiti
Thank you for the feedback.
This is an issue and it will be fixed in the next CubeMX release.
Best Regards,
Khouloud.
2019-03-20 2:04 AM
Thanks Khouloud,
Great to hear it's not a limitation of the smaller package/pinmux. We'll code around the issue for now and look forward to the next CubeMX release.
Best regards, Kieran.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.