2019-10-31 2:30 AM
Hello
some LL DMA commands do not work correctly.
CubeMX generates the following SPI/DMA init code:
...
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* SPI2 DMA Init */
/* SPI2_TX Init */
LL_DMA_SetPeriphRequest(DMA1, LL_DMA_CHANNEL_5, LL_DMA_REQUEST_1);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_5,
LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PRIORITY_LOW);
LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_5, LL_DMA_PDATAALIGN_HALFWORD);
LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_5, LL_DMA_MDATAALIGN_HALFWORD);
...I figured out that these commands don't do anything:
The values in the register DMA1->CCR5 all remain at 0.
Is this a bug or did I miss something?
I'm use the library STM32Cube FW_L4 V1.14.0 with a STM32L475RETx.
Best regards
2019-11-01 1:37 PM
> The values in the register DMA1->CCR5 all remain at 0.
Can you change them in the debugger? Is the DMA clock switched on in RCC?
JW
2019-11-04 1:11 AM
Yes, i can them change in the debugger and also when I write the values "manually" direct in the register (DMA1_CSELR->CSELR |= 1 << DMA_CSELR_C5S_Pos;).
Yes, the DMA clock is also enabled.
In the meantime, I've found out that this command works:
LL_DMA_ConfigTransfer(DMA1, LL_DMA_CHANNEL_5, LL_DMA_DIRECTION_MEMORY_TO_PERIPH |
LL_DMA_PRIORITY_HIGH | LL_DMA_MODE_NORMAL |
LL_DMA_PERIPH_NOINCREMENT | LL_DMA_MEMORY_INCREMENT |
LL_DMA_PDATAALIGN_HALFWORD | LL_DMA_PDATAALIGN_HALFWORD);Best regards
2019-11-25 1:05 AM
Is there already an explanation from STM why these commands do not work?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.