2021-07-12 4:31 PM
FlashSTM32H7xxxl_BANK1.flash operation error
I want to know the cause of this message.
Of course, it's not your program.
The above example is an example downloaded through STM32CUBEMX.
2021-07-12 4:45 PM
https://community.st.com/s/question/0D53W00000wzGplSAE/connectiion-error
So, the board and comms work Ok.
If the loader in IAR isn't working you'll need to look at those settings, as available. Perhaps if there are some dual banking settings (side-by-side, end-to-end) perhaps report those.
If TWO options for the flash, pick the OTHER setting, and see if that works. Or change the banking option bytes.
Installed available patches for IAR?
STM32Cube_FW_H7_V1.5.0\Utilities\PC_Software\IDEs_Patches\EWARM\EWARMv8_STM32H7xx_Support_V1.zip
2021-07-12 4:54 PM
STM32Cube_FW_H7_V1.8.0\Utilities\PC_Software\IDEs_Patches\EWARM\EWARMv8_STM32H74x-75x_Support_V1.6.zip
2021-07-12 9:03 PM
first . which one download? (STM32Cube_FW_H7_V1.5.0\Utilities\PC_Software\IDEs_Patches\EWARM\EWARMv8_STM32H7xx_Support_V1.zip /STM32Cube_FW_H7_V1.8.0\Utilities\PC_Software\IDEs_Patches\EWARM\EWARMv8_STM32H74x-75x_Support_V1.6.zip)
Second. how to download? I mean that I can not find both
2021-07-14 8:21 PM
I'd probably go with the latter, being newer
These are from the CubeH7 packages, usually will be in your repository directories if using CubeMX or CubeIDE, or you can select and download from the CubeH7 page on ST's site, or perhaps the files from their GitHub
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.