2017-11-29 5:41 AM
I'm trying to create a MSD for the STM32L073RZT6, and want to use 64K of the flash memory as storage.
I've tried to get the erase/write correct, but Windows says the format fails...
Can anyone spot the obvious mistake?
&sharpdefine EEPROM_START 0x8020000
&sharpdefine EEPROM_LENGTH 0x0010000
&sharpdefine STORAGE_LUN_NBR 1
&sharpdefine STORAGE_BLK_SIZ 0x200
&sharpdefine STORAGE_BLK_NBR (EEPROM_LENGTH / STORAGE_BLK_SIZ)
int8_t STORAGE_Read_FS (uint8_t lun,
uint8_t *buf, uint32_t blk_addr, uint16_t blk_len){ /* USER CODE BEGIN 6 */ uint32_t newAddr = (STORAGE_BLK_SIZ * blk_addr) +EEPROM_START; memcpy(buf, (void *) newAddr, blk_len * STORAGE_BLK_SIZ); return (USBD_OK); /* USER CODE END 6 */ }int8_t STORAGE_Write_FS (uint8_t lun,
uint8_t *buf, uint32_t blk_addr, uint16_t blk_len){ /* USER CODE BEGIN 7 */ FLASH_EraseInitTypeDef eraseInfo; uint32_t PageError; HAL_FLASH_Unlock(); // 128 byte pages in our flash, so 4 pages per storage block - erase the blocks eraseInfo.TypeErase = FLASH_TYPEERASE_PAGES; eraseInfo.PageAddress = EEPROM_START + blk_addr * (STORAGE_BLK_SIZ / FLASH_PAGE_SIZE); eraseInfo.NbPages = blk_len * (STORAGE_BLK_SIZ / FLASH_PAGE_SIZE); HAL_FLASHEx_Erase(&eraseInfo, &PageError);for (int a = 0; a < (blk_len * STORAGE_BLK_SIZ); a += 4)
{ HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, EEPROM_START + (blk_addr * STORAGE_BLK_SIZ) +a , *((uint32_t *)&buf[a])); }HAL_FLASH_Lock();
return (USBD_OK); /* USER CODE END 7 */ }#cubemx #msd2017-11-29 6:08 AM
Do any of the functions throw error or status you might be ignoring?
2017-11-29 9:26 AM
One bug I have noticed:
eraseInfo.PageAddress = EEPROM_START + blk_addr * (STORAGE_BLK_SIZ / FLASH_PAGE_SIZE);
should be:
eraseInfo.PageAddress = EEPROM_START + (blk_addr * STORAGE_BLK_SIZ);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.