2024-09-12 6:20 AM - last edited on 2024-09-13 6:33 AM by Andrew Neil
Dear @KDJEM.1 ,
I have seen that in STM32CubeIDE Version: 1.16.0 this issue is solved if the "Generate peripheral inizialization as a pair of '.c/.h' files per peripheral" is NOT selected in the ".ioc". Otherwise, the problem keeps there and "HAL_PWREx_EnableVddUSB()" is not called.
Here, you can see the code if the option is NOT selected:
void HAL_PCD_MspInit(PCD_HandleTypeDef* hpcd)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(hpcd->Instance==USB_DRD_FS)
{
/* USER CODE BEGIN USB_DRD_FS_MspInit 0 */
/* USER CODE END USB_DRD_FS_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* Enable VDDUSB */
HAL_PWREx_EnableVddUSB();
/* Peripheral clock enable */
__HAL_RCC_USB_CLK_ENABLE();
/* USB_DRD_FS interrupt Init */
HAL_NVIC_SetPriority(USB_DRD_FS_IRQn, 6, 0);
HAL_NVIC_EnableIRQ(USB_DRD_FS_IRQn);
/* USER CODE BEGIN USB_DRD_FS_MspInit 1 */
/* USER CODE END USB_DRD_FS_MspInit 1 */
}
}
And here if the option is selected:
void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(pcdHandle->Instance==USB_DRD_FS)
{
/* USER CODE BEGIN USB_DRD_FS_MspInit 0 */
/* USER CODE END USB_DRD_FS_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* USB_DRD_FS clock enable */
__HAL_RCC_USB_CLK_ENABLE();
/* USB_DRD_FS interrupt Init */
HAL_NVIC_SetPriority(USB_DRD_FS_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USB_DRD_FS_IRQn);
/* USER CODE BEGIN USB_DRD_FS_MspInit 1 */
/* USER CODE END USB_DRD_FS_MspInit 1 */
}
}
As you can observe, in the second case, the function is missing.
Could you please check that?
In my case, the selected uC is STM32H563ZIT6.
Thank you and regards.
Egoitz.
Solved! Go to Solution.
2025-03-06 12:55 AM
Hello all;
The issue is fixed in STM32CubeIDE 1.18.0 version and STM32cubeMX 6.14.0 version.
Could you please try with latest versions of STM32CubeIDE and/or STM32CubeMX and let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-12 7:40 AM - edited 2025-04-07 8:58 AM
Hello @ego ,
This post is moved from Solved:STM32H573 USBX CDC ACM(DEVICE) - STMicroelectronics Community.
Thank you for bringing this issue to our attention.
I confirm the issue HAL_PWREx_EnableVddUSB() function call is not generated at any source code in the project when generating code by choosing "Generate peripheral initialization as a pair of '.c/.h' files per peripheral"
I reported this issue internally.
Internal ticket number: 190972 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-12 9:12 PM
Great, thank you Kaouthar!
Best regards.
2024-10-29 6:33 PM
After spending most of an evening pulling my hair out, unable to figure out why I couldn't get USB to work on the STM32H523, I eventually found this same issue.
Without
being called, the USB interrupt never fires, thus breaking USB entirely.
I'm posting primarily to get this into Google's index in case others have the same issue.
2024-11-28 4:12 PM
Hi,
I also ran into the same problem, unfortunately after two weeks of searching... STM32H523 microcontroller, CubeIDE updated today to version 1.17, unfortunately still no changes.
Manually adding a call to the HAL_PWREx_EnableVddUSB() function solves the problem, but this is only a temporary solution, because the added code fragments disappear after re-generating the code from CubeMX.
I hope the problem can be solved quickly.
2025-03-06 12:55 AM
Hello all;
The issue is fixed in STM32CubeIDE 1.18.0 version and STM32cubeMX 6.14.0 version.
Could you please try with latest versions of STM32CubeIDE and/or STM32CubeMX and let me know if the issue is solved or not?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-04 3:01 AM
Hi,
The issue is NOT fixed in STM32CubeIDE 1.18.0 version when I start with STM32H503RBT6 USB.
2025-04-07 6:54 PM
Once the HAL_PWREx_EnableVddUSB() is added did you only get an interrupt when a USB device (such as a flash drive) is inserted/removed? I get constant interrupts on the STM32H563 once this is added and interrupts are enabled.
2025-04-07 6:59 PM
With all the examples I've implemented once the HAL_PWREx_EnableVddUSB() is added and interrupts enabled (__HAL_HCD_ENABLE) in HAL_HCD_Start() I get constant interrupts for the USB that blocks all other operations. Shouldn't I only get an interrupt when a USB device (such as a flash drive) is inserted/removed? I cannot understand why this is happening after looking at several USB Host examples for MSC Host project (for the STM32H563) and Dual Class MSC and HID project for the STM32H573 both provided by ST.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.