cancel
Showing results for 
Search instead for 
Did you mean: 

Misalignment between STM32CubeMX and the datasheet of STM32G030J6 regarding USART modules

AShap.5
Associate II

I am interested in how many USART modules are available in the STM32G030J6.

Datasheet contains contradictions.

According to table 12 (pages 32-34) we get the following:

USART1_TX 8 pin

USART1_RX 1 pin

USART2_TX 4 pin

USART2_RX 8 pin

According to Figure 6 (page 30) and Table 13 (page 35) we get the following:

USART1_TX 5 pin

USART1_RX 1 pin

USART2_TX 4 pin

USART2_RX 8 pin

STM32CubeMX indicates that only USART1 is available.

How right?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6

Hi. Only one USART in the STM32G030J6. Pin "PA8/PA11[PA9]/PB0/PB1" don`t have  USART1_TX.

AShap.5
Associate II

STM32CubeMX make this:

0690X00000AQPapQAH.png

Pin "PA8/PA11[PA9]/PB0/PB1" have USART1_TX

How right?

What is your CubeMX Version?

0690X00000AQQoEQAX.png

Last version - 5.3.0

1st step:

0690X00000AQSo6QAH.png

2nd step

0690X00000AQSoBQAX.png

Amel NASRI
ST Employee

Hello @AShap.5​ ,

This seems to be a limitation on STM32CubeMX side as it is possible to use USART2 on pins 4 and 8 of STM32G030Jx SO8N package.

This will be reported to our STM32CubeMX team.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @AShap.5​ 

Thanks for the feedback,

 It will be fixed in the next CubeMX release.

Regards,

Nesrine

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.