2025-07-15 5:55 AM - edited 2025-07-15 6:11 AM
In my project for an STM32H7S3, I have a number of GPIO settings.
However, every time I open the file, one particular pin has its settings reverted to the defaults.
Also, if I save the IOC file without making any changes at all, I can see in the diff that the settings for that pin have been removed:
I'm currently using Cube 6.15.0, though this file was created with an earlier version.
I'm not willing to share my IOC file here, though I'd be happy to send it privately to someone at ST.
(See also another post by me about settings being lost without any action on my part.)
Thank you.
2025-07-18 6:19 AM
Hello @Steve Melnikoff ,
Do you have the same behavior with other MCUs (or only when selecting STM32H7S3)?
Please share in private your ioc file that will help us to reproduce the issue.
2025-07-18 6:35 AM
> Do you have the same behavior with other MCUs (or only when selecting STM32H7S3)?
I'm afraid I haven't tried it with any other MCUs.
> Please share in private your ioc file that will help us to reproduce the issue.
I've sent it to @Ghofrane GSOURI . Would you be able to get it from them?
Many thanks.
2025-07-18 7:13 AM
I escalated your issue internally to CubeMX team for analysis (via internal ticket number 214422)
(PS: Internal ticket number 214422, is an internal tracking number and is not available outside of ST)
2025-08-04 6:40 AM
Hello @Steve Melnikoff ,
I am not able to reproduce the described behavior.
Do you have the same issue with different MCUs?
2025-08-04 6:44 AM
Hello.
I have not tried it with any other MCUs.
Can you confirm that you have:
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.