cancel
Showing results for 
Search instead for 
Did you mean: 

I am using the stm32g473mbt I generate a project with cube mx I only confirm the communication with the 5-pin jtag, from the main I read Systiks timer, with the library running_boot1 = HAL_GetTick (); i the reading is always 0

Dsaba.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

If SysTick isn't being called, perhaps you have interrupts disabled. Hard to know what's going on without any code.

If you feel a post has answered your question, please click "Accept as Solution".
Paul1
Lead

Has this function been generated by MX: SysTick_Handler()

It calls HAL_IncTick() which is the counter returned by HAL_GetTick()

Should be enabled in MX:

  • Pinout & Config > System Core > NVIC > NVIC > Time base > Ensure its enabled
  • Pinout & Config > System Core > NVIC > Code Generation > Time base > Ensure [Generate IRQ Handler] and [Call HAL handler] are enabled
  • If they aren't all enabled try to figure out how that happened, as I think these are enabled by default in new projects.

Paul

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.