2020-08-24 11:50 PM
I want to a project from the scratch using the STM32CubeIDE for a STM32 Nucleo board. But I don't want to use the CubeMX feature of the IDE. I just to use the HAL libraries like we can do Ac6 workbench software. In Ac6 software, we have an option to use the SPL or HAL library to build the code, can't we do in this IDE also, with just the use of HAL library not MX thing.
TIA.
Solved! Go to Solution.
2020-08-25 5:42 AM
You can create a new STM32 project as usual and delete the .ioc file. No more code generation.
Alternatively, you can select Targeted Project Type: Empty during STM32 project creation.
In both cases you have to select a target chip first. This is needed for generating the right linker description file etc..
Drivers (CMSIS + HAL + LL) are available separately in the STMCube packages. You can mix them in as needed.
2020-08-25 5:42 AM
You can create a new STM32 project as usual and delete the .ioc file. No more code generation.
Alternatively, you can select Targeted Project Type: Empty during STM32 project creation.
In both cases you have to select a target chip first. This is needed for generating the right linker description file etc..
Drivers (CMSIS + HAL + LL) are available separately in the STMCube packages. You can mix them in as needed.
2020-08-25 8:57 PM
Thank you @KnarfB. It worked.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.