2016-05-02 2:01 AM
Dear all,
Actually we are designing a hardware using STM32f407VGT6 micro-controller, already we are accessing this hardware with usb, but in addition we want Ethernet based communication to operate that hardware(access data and control both), so we start to test it first on STM32F4 Discovery kit and Base Board.We download demo code for Http Server using LWIP Stack and run it using Keil ide, the demo code working fine, we were unable to access that web application using IP, that is code to microcontroller.But when we are trying to create a code using STM32CubeMX, it only create lwip code not Http Server code.We don't want to run or use democode, that was ok only for initial demo, now we want to create own using STM32Cube Mx and Keil.So plz anyone help us in this project guide us, ''How to develop Http server application on STM32F4 Discovery Board using STM32CubeMX and Keil''Thank you MembersRegards,Mohit #lwip #stm32cubemx #stm32cubemx #stm32f4 #stm32f4 #!stm32f4 #discovery #discovery #!stm32f42016-05-02 10:20 AM
Hi,
I'd recommend you to have a look to the paragraph B.3.6 LwIP in the User manual.Regards2016-05-03 12:07 AM
Hello forumstm32,
First of all thank you for reply.I check that PDF file and we already apply, that is given in this.Actually, when we try to run demo(downloaded form st or keil website), its working fine.We got output on screen using web browser by access ip 192.168.0.10 (i.e. asign to microcontroller), like this as showing in this videoBut when we are generating the code through STM32CubeMX, it consist only lwip stack middleware library, not have web code or folder that should be access through web browser, i mean that generated code not consist the Html files folder.So how can we create that, any idea?Thank youRegards,Mohit2016-05-03 5:48 AM
Cube is just a framework tool, it is not going to create complicated applications.
You'd want to look at how the other ETH/LwIP examples in-line a file system. Specifically the use of tools to create .C/.H files encapsulating files in a directory.2016-08-04 9:07 AM
2016-08-04 12:29 PM
I'm an Electronics Engineer
The tool, or script, in question is makefsdatahttps://github.com/goertzenator/lwip/tree/master/contrib-1.4.0/apps/httpserver_raw/makefsdata
A quick Google found a Windows GUI tool for doing this.http://developers.stf12.net/Ethernet-demo/latest-news/Added-Makefsdata-utility
It is a basically tool that navigates a sub-directory, and outputs .C and .H files, as required, to describe the data in a way that can be compiled into the application. The abstraction is managed by the FS.C code, which emulates open, close, read interfaces to the file system encapsulated in the creation step.To read files off an SD Card would require replacing some or all of the file system layer of the web server.2016-10-07 8:33 AM
Dear Mohit,
You can use the example code provided as reference into STM32Cube firmware package.
STM32CubeMX has downloaded this package to a repository folder on your PC (Check updater settings for repository location): go to the project directory, then to the EVAL board directory, and application folder. There you'll find LwIP examples such as the ''LwIP_HTTP_Server_Netconn_RTOS'' example project.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.