2020-07-09 2:10 PM
Hi,
I have read the STM32F303RE reference manual along with using CubeMX 5.6.1 but can't seem to do what I want. The documentation of CubeMX is less than desirable IMHO.
As an aside I am already using TIM2_CH2 on pin PB3 in Input Capture Direct Mode and using this to generate a DMA request. This is working.
Now I want COMP7 to use DAC1_CH1 on the inv input and use pin PC1 on the non-inverting input. Then I want COMP7 output to go to TIM2_IC3.
I'm unclear how to set up TIM2_CH3 in this scenario. When I select Input Capture Direct Mode CubeMX automatically chooses pin PB10 as TIM2_Ch3. I don't want an external pin selected, I want the COMP7 output.
In CubeMX for TIM2 what do I choose as the mode for Ch3 ?
2020-07-09 9:15 PM
The input from GPIO matrix is ORed with the comparator signal.
If you don't set any pin to given channel, that input is probably 0, but that's not confirmed by ST,
I don't care how to do that in CubeMX, I don't use it.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.