2019-02-07 11:32 PM
Hello,
I need to receive UDP Broadcast, but The "callback" function is never called.
"No broadcast" UDP communication works fine.
Is IwIP at all able to receive UDP broadcast?
I use LwIP 2.0.3, STM32F407, PHY DP83848
/*----- Default Value for IP_SOF_BROADCAST: 0 ---*/
#define IP_SOF_BROADCAST 1
/*----- Default Value for IP_SOF_BROADCAST_RECV: 0 ---*/
#define IP_SOF_BROADCAST_RECV 1
void udp_server_init(void)
{
struct udp_pcb *upcb;
err_t err;
upcb = udp_new();
ip_set_option(upcb, SOF_BROADCAST);
if (upcb)
{
err = udp_bind(upcb, IP_ADDR_BROADCAST, 8000);
if(err == ERR_OK)
{
udp_recv(upcb, udp_receive_callback, NULL);
}
}
}
void udp_receive_callback(void *arg, struct udp_pcb *upcb, struct pbuf *p, const ip_addr_t *addr, u16_t port)
{
HAL_GPIO_TogglePin(GPIOE, GPIO_PIN_2);
pbuf_free(p); // Free the p buffer
//udp_transmit(upcb, addr, udp2_tx_data, udp2_tx_len);
} Thank you
Peter
2019-02-08 4:16 AM
DHCP client in dhcp.c uses IP4_ADDR_ANY. Maybe try binding to that for the sake of experiment.
Check BFD bit in ETH->MACFFR and maybe try RA bit.
Also make sure that NETIF_FLAG_BROADCAST flag is set for netif->flags.
2019-02-08 7:12 AM
Hi Piranha,
NETIF_FLAG_BROADCAST is enabled in: static void low_level_init(struct netif *netif)
static void low_level_init(struct netif *netif)
{
....
/* Accept broadcast address and ARP traffic */
/* don't set NETIF_FLAG_ETHARP if this device is not an ethernet one */
#if LWIP_ARP
netif->flags |= NETIF_FLAG_BROADCAST | NETIF_FLAG_ETHARP;
#else
netif->flags |= NETIF_FLAG_BROADCAST;
#endif /* LWIP_ARP */
...
}I tried too: err = udp_bind(upcb, IP_ADDR_BROADCAST, 8000);
I use MX_LWIP_Init() which it generates by STM32CubeMx.
It still doesn't work.
Peter
2019-02-08 3:28 PM
https://www.nongnu.org/lwip/2_0_x/group__udp__raw.html#gac7fbda8b12b9b9360e92b51e805e799e
"ipaddr - local IP address to bind with. Use IP4_ADDR_ANY to bind to all local interfaces."
It's the local address of network interface to which binding must be done. It can't be IP_ADDR_BROADCAST as broadcast address is not a local address.
2019-02-09 1:31 AM
Some additional information. IP_SOF_BROADCAST and IP_SOF_BROADCAST_RECV enables broadcast filtering per connection. By default those are off and that means that all connections receive broadcasts irrespective of SOF_BROADCAST. When per connection filtering is enabled, no connection receives broadcasts unless SOF_BROADCAST option is set for particular connection.
2024-10-23 2:41 PM - edited 2024-10-23 2:48 PM
I am trying to receive a message using the many broadcast IPs (192.168.1.255, IP_ADDR_BROADCAST, and also (0, 0, 0, 0)). None seemed to work. My network mask is (255.255.255.0).
Initially, I installed a PCB that already works. I tried the attempt below, but it did not work.
int UdpCommunication::ResetUdpBroadcast() {
ip_addr_t broadcast_ip_address_v4;
IP4_ADDR(&broadcast_ip_address_v4, 0, 0, 0, 0); // Bind to IP_ADDR_ANY
udp_remove(udp_pcb_broadcast_);
udp_pcb_broadcast_ = udp_new();
ip_set_option(udp_pcb_broadcast_, SOF_BROADCAST);
auto lwip_error = udp_bind(udp_pcb_broadcast_, &broadcast_ip_address_v4, 10999);
if (lwip_error != ERR_OK) {
udp_remove(udp_pcb_broadcast_);
return 1;
}
udp_recv(udp_pcb_broadcast_, UdpCommunication::UdpReceivedCallback, this);
return 0;
}
Is there any hint or extra documentation on this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.