2022-01-18 3:15 AM
There is a bug in the CubeMX Code Generation in STM32CubeIDE Code Generation (Version 1.7.0 updated to 1.8.0) for the STM32F767ZI. (STM32Cube FW_F7 V1.16.2)
The bug was found by debugging a not working auto generated code that is using a DMA circular buffer to read from uart.
In the auto generated initialization code for the hardware the ordering of the function calls was:
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_DMA_Init();Because DMA_Init starts the clock to the dma the dma isn't clocked when initializing the uart which uses the DMA.
This leads to a non functioning dma transfer and the uart overflow error is triggered because nothing is reading from the uart peripheral.
As a work arround you can write:
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);before the block with the MX initializiation functions or you can swap the calls to dma init and uart init.
Solved! Go to Solution.
2022-01-18 3:25 AM
Hello @PKrem.1 ,
First let me thank you for having reported.
when DMA is used, the MX_DMA_Init shall always be called before any other HAL_***_Init (where *** is any peripheral with a HW dependency on DMA init code).
A regression was detected in the previous STM32CubeMX version 6.3.0 (STM32CubeIDE Version: 1.7.0 ) generating a wrong order of initialization functions, and it seems to be corrected for some use cases.
For example, starting a project from scratch and configuring I2S and DMA in one shot (without switching to Project Manager view before configuring I2S DMA request), MX_DMA_Init Function call will be in its correct position.
With this being said, and as mentioned by @Javier Muñoz , you can refer to the this post proposing a workaround to overcome this issue: re-order initialization functions through Project Manager view > Advanced Settings tab.
Hope this clarifies the situation.
Khouloud.
2022-01-18 3:19 AM
This is a known issue, cubeMX generates the init function in the wrong order.
@Amel NASRI pointed me to https://community.st.com/s/question/0D53W00001EzCmCSAV/mxdmainit-order-in-the-mainc-file-generated-by-stm32cubemx-how-to-fix
2022-01-18 3:25 AM
Hello @PKrem.1 ,
First let me thank you for having reported.
when DMA is used, the MX_DMA_Init shall always be called before any other HAL_***_Init (where *** is any peripheral with a HW dependency on DMA init code).
A regression was detected in the previous STM32CubeMX version 6.3.0 (STM32CubeIDE Version: 1.7.0 ) generating a wrong order of initialization functions, and it seems to be corrected for some use cases.
For example, starting a project from scratch and configuring I2S and DMA in one shot (without switching to Project Manager view before configuring I2S DMA request), MX_DMA_Init Function call will be in its correct position.
With this being said, and as mentioned by @Javier Muñoz , you can refer to the this post proposing a workaround to overcome this issue: re-order initialization functions through Project Manager view > Advanced Settings tab.
Hope this clarifies the situation.
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.