2024-11-07 6:21 AM
It is a very common practice the source files go in pairs: a .h file with the interface, and a .c file with the implementation.
This is acknowledged in CubeMX - which has an option to do exactly that:
But, with CubeIDE (in fact, Eclipse), it requires a 2-step process:
Feature Request: add an option to create a pair of files - .c and .h - in one go.
2024-11-07 8:02 AM
Hello @Andrew Neil ,
First let me thank you for posting.
I've escalated the request to the concerned team (under internal ticket number 195933).
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-11 2:38 AM - edited 2024-11-11 8:36 AM
Thanks - I'll look forward to it ...
As it's not actually solved yet, I won't mark a solution yet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.