2023-11-09 6:56 AM
Dear Sir and Madam,
I started a new project with STM32H745 from scratch. After implementation of all pin function and names, I worked on the clock tree. During this, I saw, one UART must be changed to the FDCAN interface. While doing this, CubeMX was getting frozen. Killing CubeMX and open the same file again show me the error
Doing the same on a PC from a colleague runs in the same trouble.
The projectfile and the message is atteched. If someone able to reconstruct my file?
I use CubeMX Version 6.9.2 under Windows 11
Thanks,
Jan
Solved! Go to Solution.
2023-11-09 8:17 AM
Well, if I comment out lines 1007 and 1008 (containing the string USB_OTG_FS.) with a preceding # in your IOC, it can be loaded successfully. However, it looks like the USB configuration information has been corrupted.
Maybe this will help you as a starting point?
Regards
/Peter
2023-11-09 8:04 AM
Hello @JPiet.3
Can you please provide more details about the steps you followed in order to reproduce your issue.
Thank you,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-09 8:10 AM
Not complete in detail, but the following last step I keeped in mind.
I wanted to change the pin-function from UART to FDCAN (PINS PH13, PH14). When I was switching to the categories connectivity, no click with the mouse button was recognized. After different tries, I killed CubeMX to start it again.
2023-11-09 8:17 AM
Well, if I comment out lines 1007 and 1008 (containing the string USB_OTG_FS.) with a preceding # in your IOC, it can be loaded successfully. However, it looks like the USB configuration information has been corrupted.
Maybe this will help you as a starting point?
Regards
/Peter
2023-11-09 11:26 PM
Thanks a lot, it works. Good to know, it is not necessary to rebuild the complete project :)
Jan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.