cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 6.0.0, STM32F412RE, SDIO, 4 Bit, DMA - Reinitialisation of uSD makes problems

MarieMaurer
Associate III

I have meanwhile a running uSD card. I have the need to reinitialize the card.

In FatFS I do an unmount (it is a mount with certain parameters).

It looks like the following is missing:

void MX_FATFS_DeInit(void)

{

/*## FatFS: UnLink the SD driver ###########################*/

retSD = FATFS_UnLinkDriver(SDPath);

/* USER CODE BEGIN Init */

/* additional user code for init */

/* USER CODE END Init */

}

But now when I reinit the SDIO, it looks like there is a hen-and-egg-problem:

SD_WideBus_Enable / SD_WideBus_Disable

uses SD_FindSCR to get supported bus wide modes.

SD_FindSCR calls

SDMMC_CmdSendSCR

which configures how to transfers data over DAT0 or DAT0 to DAT3 lines (depending on the previous configuration of SDIO bus width). I am not completely sure, if I am correct.

I know or I can store if I was at 4 bit wide mode, but if SDIO bus wide does not fit uSD bus wide, I cannot switch to be able to communicate again.

I don't know yet how to solve it.

Is there perhaps something like

SD_deinitialize

needed in

const Diskio_drvTypeDef SD_Driver = { ... };

?

Going one step back it is perhaps a bad idea to use a command to read supported bus width,

with a command which is dependant on the bus width. Is there perhaps some command to get actual bus width without using any DATx lines? Or can I force card to 1 bit bus width, some "force initialisation" using only CMD communication when I can't control power of the uSD card?

Some special cases:

1) User takes card out and reinserts it. I don't want to power cycle the device. I want to (re-)access the uSD after inserting.

( uSD was without power and resetted all previous configuration settings )

2) uC is doing a SW reset (e.g. firmware update with a reset to restart, hard fault with restart, ...)

( uSD has still power, remains at current settings, but uC is doing a new startup)

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.